NXP’s i.MX RT Crossover Processor Sets Highest Microcontroller Real-Time Benchmark Performance Yet
Industry’s first crossover processor based on ARM® Cortex®-M7 delivers a CoreMark score of 3020, DMIPS of 1284 and 20ns interrupt latency at 600 MHz – Available now and priced at a fraction of the cost of competing solutions

SANTA CLARA, Calif., Oct. 24, 2017 (GLOBE NEWSWIRE) -- (ARM TECHCON 2017) -- NXP Semiconductors N.V. (NASDAQ:NXPI) presents the i.MX RT series, a crossover solution that bridges the gap between high performance and integration while minimizing costs. As the need for smarter and more ‘aware’ edge computing grows and becomes critical to the development of the Internet of Things (IoT), edge devices are expected to provide the highest compute performance together with reliable security and assured privacy at the lowest cost possible. These essential capabilities with enablers like graphics and display support and seamless connectivity increase system-level costs and extend time-to-market.

NXP i.MX RT Crossover Processor
NXP’s i.MX RT Crossover Processor Sets Highest MCU Real-Time Benchmark Performance Yet – Industry’s first crossover processor based on Arm Cortex-M7 delivers a CoreMark score of 3020, DMIPS of 1284 and 20ns interrupt latency at 600 MHz – Available now and priced at a fraction of the cost of competing solutions


A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/b5a14333-e107-4e03-998e-5c98b37647f3

NXP tackles this challenge by architecting i.MX RT crossover processors to deliver high performance and functional capabilities of applications processors, but with the ease-of-use and real-time deterministic operation of traditional microcontrollers (MCUs). Ideal applications include audio subsystems, consumer and healthcare, home and building automation, industrial computing, motor control and power conversion.

The new crossover processors offer high levels of integration and rich user experiences (graphics, display, and audio) while reducing system-level costs. The i.MX RT with high-density Static Random-Access Memory (SRAM) and integrated DC-DC delivers unprecedented performance per dollar. The inclusion of fast and secure interfaces for external memories eliminate the need for embedded flash, thus reducing product costs and significantly lowering the cost of flash programming.

“We see embedded designers being forced to make trade-offs between performance and cost in their end products. The i.MX RT’s impressive leap in both areas is indicative of NXP’s innovation and understanding of real market needs,” said Markus Levy, President of EEMBC. “This kind of unique approach will revolutionize embedded designs across ‘thousands’ of IoT applications.”

Performance and Power Comparisons

The new i.MX RT1050 is the highest performing ARM Cortex-M7 based device with real-time operation and an applications processor-level of functionality. At 600 MHz, it is 50 percent faster than any other Cortex-M7 product and more than two times faster than existing Cortex-M4 products. By combining this high performance with a Cortex-M7 core, an interrupt latency as low as 20 nanoseconds – the lowest among all ARM Cortex-based products in the world has been achieved. Furthermore, by integrating 512KB of Tightly Coupled Memory (TCM) SRAM, a very high effective core performance is maintained for real-time IoT applications.

An integrated DC-DC converter not only eliminates a need for an external PMIC, but also enables an active power efficiency (CoreMark per mW) that is 2-4x better than competing MCU solutions.  At 110 μA/MHz (full operation) the i.MX RT1050 is 2-3x better than the competing Cortex-M7 based MCUs.

Integration and Ease of Use

The i.MX RT1050 enables advanced GUIs, enhanced HMIs and greater design flexibility with multiple external memory interface options. High security embedded designs are made possible by high-efficiency encryption engine for AES-128, High Assurance Boot (HAB) and On-the-fly QSPI Flash Decryption.

MCU customers can leverage their current toolchain including MCUXpresso Software and Tools, IAR Systems and ARM Keil MDK saving time and tool reuse. Rapid developing and easy prototyping are possible with open source real-time operating systems including FreeRTOS, ARM Mbed™ OS, Zephyr™ OS, and the global ARM ecosystem that provides software libraries, online tools, and support. Using the low-cost evaluation kit (EVK) compatible with Arduino™ hardware shields enables faster development. And, NXP’s ready-to-play USB Type-C shield board works with i.MX RT through the Arduino header to further ease development.

“RT blows the lid off anything else on the market. It enables customers to move up to application-level performance while staying with their current tool-chain and ecosystems. It’s also much easier on the supply chain to program low pin count serial flash than a wide variety of larger package MCUs,” said Geoff Lees, senior vice president and general manager of microcontrollers at NXP. “Stay tuned, the race to GHz Cortex-M is on.”

Pricing and Availability

Best of all, the leading performance and power efficiency of the i.MX RT series comes at an affordable price. And, BOM cost reductions are achieved with 2-4 layer PCB design and savings can be realized by programming external flash as compared to programming flash on-chip on a large MCU.

Two families have been introduced for maximum flexibility with features, pricing, and packaging.

  • i.MX RT1050 is available now starting at $2.98 USD for 10K quantity
  • i.MX RT1020 will be available Q2 2018 and priced at $2.18 USD for 10K quantity

Presence at ARM TechCon

  • Experience the audio playback demo powered by i.MX RT at NXP’s booth (#500).
  • Attend the session Wed, Oct 25 at 11:30 am: The Convergence of Applications Processors and Microcontrollers Unfolds with the Advent of High-Performance ARM Cortex-M7 Based Devices

About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 31,000 employees in more than 33 countries and posted revenue of $9.5 billion in 2016. Find out more at www.nxp.com.

NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. ARM and Cortex are trademarks or registered trademarks of ARM Ltd or its subsidiaries in the EU and/or elsewhere. All rights reserved. © 2017 NXP B.V.

For more information, please contact:      

Americas
Tate Tran
Tel: +1 408 802 0602
Email: tate.tran@nxp.com

Greater China/Asia
Esther Chang
Tel: +886 2 8170 9990
Email: esther.chan@nxp.com

Europe
Martijn van der Linden
Phone: +31 6 1091 4896
Email: martijn.van.der.linden@nxp.com 

Primary Logo

NXP Semiconductors N.V.