Press Release

NXP Strengthens Industrial Connectivity Portfolio with Multi-Protocol Sub-GHz Wireless Transceiver Platform

BARCELONA, Spain, Nov. 16, 2016 - NXP Semiconductors today launched the OL2385 family of turnkey sub-GHz wireless transceivers, adding to its industry leading, low-power microcontroller and 2.4 GHz portfolio for IoT applications. This portfolio combines scalable computing, wireless connectivity, embedded security, sensors and software to provide integrated solutions for low-power, industrial IoT applications.


The OL2385 is based on a PIN-to-PIN compatible sub-GHz transceiver hardware platform and supports multiple wireless protocols such as Sigfox, W-MBus powered by Xemex and ZigBee® IEEE 802.15.4. The transceivers combine excellent RF performance with low-power consumption making it ideal for battery powered applications such as home and building automation, smart metering as well as asset tracking and monitoring. The platform is designed to shorten design cycles with NXP software stacks tested for standards compliance and delivered with pre-certified binaries.


"Sigfox is pleased to have NXP Semiconductors join the ecosystem to provide our customers even more choice of software and hardware platforms," said Tony Francesca, vice president of global ecosystem partners, Sigfox. "The OL2385 reference design is Sigfox verified having very good performance with outstanding receive sensitivity. The new NXP transceivers are optimized solutions for global module manufacturers such as Innocomm to deliver ultra-low cost IoT modules that will fuel the IoT mass-market deployment."


Andrew Chien, vice president of business development, Innocomm added, "With our Sigfox verified modules based on the OL2385, we are able to shorten the IoT device maker development cycle significantly while providing connectivity to the Sigfox network globally."


A two-way RF channel and common modulation schemes for networking applications allow the OL2385 family of transceivers to cover a full range of frequency bands from 160 to 960 MHz. Its extended range radio operation is enabled with high sensitivity, up to -128 dBm, while its operation in congested environments is enhanced with 60 dB at 1 MHz of blocking performance and 60 dB of image rejection that is best in class by approximately 10 dB. Specifically, the challenges of radio compliance in more complex applications like W-MBus and ZigBee 868 have been addressed in this device.


Gert-Jan van der Hurk, managing director of Xemex noted "We completed extensive testing of OL2385 for its suitability for W-MBus compliance, confirming that it satisfies the specification in the different modes and that we can offer our W-MBus stack with the device." Additional platform features:


  • 14 dbm Tx output power compliant with ETSI limits

  • Typical 29 mA transmit power consumption at full output power

  • Less than 11 mA receive power consumption

  • Excellent phase noise of -127 dBc at 1 MHz in the 868 and 915 MHz band for flexibility with external power amplifiers

  • Japanese ARIB T108 standard compliant


Combined with Kinetis MCUs and LPC SDK pre-developed SPI/ UART drivers, the OL2385 is a solution that offers the broadest choice of ARM® based MCUs with integrated peripherals on the market today, with fewer constraints:


  • No fast polling on SPI compared to the simplest transceiver devices without integrated MCU

  • Network stack and optimized radio setup preconfigured for the standards supported


Availability


The hardware and software for the OL2385 platform is provided in a one-stop-shop concept, with components supplied by NXP. The OL2385 platform samples and development boards with SIGFOX are available now through your sales representative. Mass production of pre-programmed parts are scheduled to start at the end of Q4/2017. The W-MBus software is readily available for evaluation and IEEE802.15.4 compliant samples are expected to become available in Q2 2017. W-MBus and IEEE802.15.4 preprogrammed parts are scheduled to become available for mass market in the 2nd quarter of 2017.


About NXP
NXP Semiconductors N.V. (NASDAQ: NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 44,000 employees in more than 35 countries and posted revenue of $6.1 billion in 2015. Find out more at www.nxp.com.


NXP the NXP logo and Kinetis are trademarks of NXP B.V. All other product or service names are the property of their respective owners. ARM is a registered trademark of ARM Limited (or its subsidiaries) in the EU and/or elsewhere. All rights reserved. All rights reserved. © 2016 NXP B.V.


For more information, please contact:        


Europe

 

 

 

 

Martijn van der Linden

 

 

 

 

Tel: +31 6 10914896

 

 

 

 

Email: martijn.van.der.linden@nxp.com

 

 

 

 


 


Published

November 16, 2016
Receive News Alerts