Press Release

NXP Unveils the Future with Innovative Security, IoT, and Automotive Solutions at CES 2017

LAS VEGAS, Jan. 04, 2017 (GLOBE NEWSWIRE) -- (CES 2017) – At this week’s CES 2017 exhibition and conference, NXP Semiconductors N.V. (NASDAQ:NXPI) will showcase how top global developers can deliver a future where everything is secure, smart, and connected. From new solutions to new partnerships, NXP is spearheading innovation for security, the Internet of Things (IoT), and automotive. 

NXP announcements at CES include:

New Collaborations to Build the Secure, Connected Ecosystem for Cars and Devices

  • At CES 2017, NXP announced it will advance security for the IoT with Microsoft. The solutions will be demonstrated at CES and combine the best of hard- and software security with other capabilities such as voice control and self-learning algorithms, for use in smart homes, connected cars, and smart connected devices.
  • From January 4-8, Microsoft, NXP, IAV and auto mobility partners, Cubic Telecom, Esri, and Swiss Re, will showcase their collective vision of safe and secure end-to-end mobility through a highly automated driving demonstration and experience. Vehicle-to-vehicle communications will continue to gain relevance, especially in the U.S., since the U.S. Department of Transportation proposed a rule to mandate the technology in new cars.
  • The new Rinspeed “Oasis”, an ingenious self-driving electric vehicle on display in Las Vegas, will use a wealth of NXP technologies for enabling securely connected, self-driving cars, including radar “cocooning”, V2X communications, automotive NFC, NXP BlueBox Sensor Fusion, long-range RFID and many more. Advanced sensing technology allows the system to capture a 360-degree view of the vehicle’s surroundings with pinpoint precision.
  • To drive innovation for future wearable technologies, also NXP revealed results from a new R&D test bed that supports development of products and applications using embedded Secure Element (eSE) technology, which underscores the company’s ongoing commitment to invest in the future development of secure payment, transit, authentication and other services for connected devices. Some of NXP’s latest successes resulting from the test bed are highlighted by solutions developed by its partners Palago and uConekt Inc.

Breakthrough Solution in Automotive to Simplify Development

  • NXP announced the SAF4000 – the world’s first fully integrated software defined radio solution capable of covering all global broadcast audio standards, including AM/FM, DAB+, DRM(+) and HD. The new IC represents a breakthrough in simplifying the development of high-performance infotainment platforms as it combines six ICs, thus replacing today’s multi-chip solutions with a single ultra-compact RFCMOS device.

Advanced IoT Semiconductors to Meet Heightening Consumer Expectations

  • NXP introduced the i.MX 8M family of applications processors specifically designed to meet increasing audio and video system requirements for smart home and smart mobility applications. NXP’s i.MX 8M family addresses the major inflection points currently underway in streaming media: voice recognition and networked speakers in audio, and the move to 4K High Dynamic Range (HDR) and the growth of smaller, more compact form factors in video.
  • The company also introduced the new roadmap for the LPC MCU portfolio based on the LPC800 and LPC54000 series with a robust pipeline of ARM® Cortex®-M-based devices for next-generation consumer and industrial IoT applications.
  • To help make connections faster and more reliable on smartphones, tablets, wearables and small Internet of Things (IoT) devices, NXP announced its new wireless local area network (WLAN) Low Noise Amplifiers (LNA) with Integrated Switch.
    Additionally the company introduced the easiest way to add Near Field Communications (NFC) technology to Hexiwear wearable devices with the new MikroElektronika NFC click, powered by NXP. The new module is a mikroBUS™ add-on board with a versatile NFC PN7120 IC controller that makes it easy to incorporate NFC, removing barriers to adoption.

New Solutions that Bring Ultimate Convenience to Charging Devices

  • NXP unveiled the industry’s first Type-C USB solution that fully charges mobile, computing and virtual reality devices in less than an hour. The end-to-end solution is the smallest in market and includes unique rapid charging coupled with USB PD PHY for the first fully compliant Type-C Port Controller (TCPC) implementation.
  • Also at CES 2017, NXP introduced the first high-power wireless charging solution for notebooks and 2-in-1 tablets, with up to 100W of delivered power, covering a wide range of power supply requirements for this segment. At <2mm in thickness and low component count, the solution is capable of fitting into the tightest industrial design constraints. Wireless charging has been a popular addition to smartphones and other small portable electronics. Portable computing devices, however, need considerably more power than available from smartphone chargers. This new NXP solution now allows consumers to have a truly cord-free experience with notebooks and 2-in-1 tablets, even with their higher power consumption requirements.

CES Showcase and Demonstration

  • NXP will showcase more than 100 demos from the smallest microcontrollers to the complex networking infrastructure that powers the new smarter world in the Smarter World Tour truck. In addition to the truck, NXP will also have an adjoining pavilion to showcase a variety of solutions. Also, new this year, NXP will demonstrate ADAS technology at the Autonomous Vehicle Marketplace in the North Plaza.

A number of NXP experts are available throughout the show to deliver demos, comment on breaking news and brief the media and analysts on NXP technology. To book a meeting or demonstration session, please contact: nxp@hoffman.com.

About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 44,000 employees in more than 35 countries and posted revenue of $6.1 billion in 2015. Find out more at www.nxp.com.

NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere. All rights reserved. © 2017 NXP B.V.       

For more information, please contact: 

Americas
Tate Tran
Tel: +1 408-802-0602
Email: tate.tran@nxp.com

Europe / U.S.
Birgit Ahlborn
Tel: +49 170 57 46 124
Email: birgit.ahlborn@nxp.com 

Primary Logo

NXP Semiconductors Netherlands B.V.

Published

January 04, 2017
Receive News Alerts