Press Release


NXP Multi-Purpose Solution in Philippines Enables Consumers to Tap Popular beep™ Card for Payment at FamilyMart Stores and Transit Ticketing
Commuters can now use their beep cards – not just for trains, buses, but also for purchases at local FamilyMart branches

METRO MANILA, Philippines, April 19, 2017 (GLOBE NEWSWIRE) -- NXP Semiconductors N.V. (NASDAQ:NXPI), today announced it will further its collaboration with AF Payments Inc., the company behind the contactless payment cards, beep™ cards in the Philippines, to add micropayment capabilities. The popular cards commonly used for transport ticketing in the Manila Light Rail Transit System Line 1 and 2, Manila Metro Train Transit System Line 3 and popular city bus routes, can now be used to pay at the FamilyMart convenience store chain, which is the second largest chain of 24-hour convenience stores in the world.

According to Peter Maher, AF Payments Inc.’s President and CEO, since the card’s launch, more than three million beep™ cards have been sold, accumulating more than four billion Philippine peso (PHP) in transactions with 18 million taps in a single month (March 2017).

“We chose MIFARE DESFire as the platform for our beep™ card because we had a bigger picture in our mind when kicking off beep™ card for transport ticketing. Now with FamilyMart allowing cashless transactions, we are convinced that it was the right choice to provide people living in and coming to Manila a convenient contactless and cashless experience even beyond transport ticketing,” said Peter Maher from AFPI.

Additionally the beep™ card can be reloaded at FamilyMart as it is a stored value card. Due to the card’s increasing popularity many additional services are likely to follow.

“The multi-application architecture of the MIFARE DESFire product line supports the AFPI strategy to provide multi-functional smart card by on-boarding third party services from other sectors. It allows them to add value to their core offering by integrating many more useful and convenient services for their loyal customers,” said Markus Staeblein, vice president and general manager, secure mobility and retail solutions at NXP. “Furthermore, our latest product, MIFARE DESFire EV2, allows customer centric organizations to offer their customers fully cloud integrated interactive experience for content management on their smart medium over the air.”

About AF Payments Inc.
AF Payments Inc. is a consortium of Metro Pacific Investments Corp. (MPIC) and Ayala Corp. that provides contactless payment solutions in the Philippines through its integrated product and services offerings, thereby enhancing the payment transaction experience of every Filipino.

About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 31,000 employees in more than 33 countries and posted revenue of $9.5 billion in 2016. Find out more at www.nxp.com.

NXP, the NXP logo, and MIFARE are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2017 NXP B.V.

For more information, please contact:        

Americas Europe Greater China / Asia      
Tate Tran  Martijn van der Linden Esther Chang      
Tel: +1 408-802-0602 Tel: +31 6 10914896 Tel: +886 2 8170 9990      
Email: tate.tran@nxp.com  Email: martijn.van.der.linden@nxp.com  Email: esther.chang@nxp.com      

Primary Logo

NXP Semiconductors Netherlands B.V.

Published

April 19, 2017
Receive News Alerts