Press Release

NXP Pushes the Limits of Solid-State RF Energy
New Transistor Delivers 750 W CW for 915 MHz Applications

MIAMI, June 20, 2017 (GLOBE NEWSWIRE) -- IMPI ANNUAL MICROWAVE POWER SYMPOSIUM -- NXP Semiconductors N.V. (NASDAQ:NXPI), the number one supplier of RF power transistors, today announced the industry’s highest power transistor for 915 MHz applications. The MRF13750H transistor delivers 750 W continuous wave (CW), fifty percent higher than comparable products currently available on the market. Based on 50 V silicon LDMOS, this transistor extends the limits of solid-state RF generation, making the MRF13750H an attractive alternative to vacuum tubes for very high power industrial systems.

This transistor brings ease of use to microwave generator designers. It delivers exceptional precision, control and reliability compared to vacuum tube-era technologies such as magnetrons. The MRF13750H supports accurate power control over the full dynamic range from 0 to 750 W, and enables frequency shifting that helps make precise use of RF energy. It is capable of operating for decades, with minimal performance degradation over time, lowering the total cost of ownership. It operates at 50 V, for greater safety than magnetrons. Finally, the small size of a solid-state power amplifier enables redundancy and flexibility of design.

“The reliability and enhanced control features of solid-state have long been understood, but industrial system designers had difficulties combining many transistors to match the power level of magnetrons — until now,” said Pierre Piel, senior director and general manager for multi-market RF Power at NXP. “The MRF13750H delivers performance that enables industrial heating engineers to implement it in very high power systems.”

“Given the many advantages of solid-state RF energy as a highly efficient and controllable heat and power source, the RF Energy Alliance (RFEA) sees endless market opportunities for the technology to improve existing RF energy applications as well as enable new ones,” said Klaus Werner, Executive Director of the RFEA. “The capabilities of the new MRF13750H will undoubtedly accelerate the industry’s transition to solid-state RF technology.”

This new transistor is designed for industrial, scientific and medical (ISM) applications ranging from 700 to 1300 MHz, especially industrial heating/drying, curing, and material welding, as well as particle accelerators. It delivers 750 W CW at 915 MHz with 67 percent efficiency in a small 3 × 3.8 inch (7.6 × 9.7 cm) pallet.

Availability
The MRF13750H is sampling today and will be in production in December 2017. The 915 MHz CW reference circuit is available today. To access the data sheet and for more information, visit www.nxp.com/MRF13750H.  

About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 31,000 employees in more than 33 countries and posted revenue of $9.5 billion in 2016. Find out more at www.nxp.com.

NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2017 NXP B.V.

For more information, please contact:        

Americas   Greater China/Asia   Europe
Joon Knapen       Esther Chang       Martijn van der Linden
Tel: ++31619303857   Tel: +886 2 8170 9990   Phone: +31 6 1091 4896
Email: joon,knapen@nxp.com
  Email: esther.chan@nxp.com
  Email: martijn.van.der.linden@nxp.com

Primary Logo

NXP Semiconductors Netherlands B.V.

Published

June 20, 2017
Receive News Alerts