A founding member of the Linaro Networking Group, Freescale drives SDN evolution and promotes software interoperability for a smarter Internet of Tomorrow
As network operators increasingly look to SDN and NFV to increase the programmability of the world’s networks, common APIs are necessary to make data plane software interoperable across processing architectures. To meet this need, Freescale is announcing support for the ODP APIs for both ARM® and Power Architecture™ versions of its QorIQ multicore processors. The ODP APIs offer a common abstraction interface for hardware-based acceleration functions such as IPSEC and traffic management, which are implemented in Freescale’s QorIQ multicore processors and engineered to support optimal network performance and security.
“As a founding member of the Linaro Networking Group, Freescale applauds the introduction of ODP version 1.0,” said Nikolay Guenov, director of product management for Freescale’s Digital Networking group. “Freescale and its QorIQ platforms are in solid alignment with ODP, which is the optimal open-ecosystem standard for meeting the performance and efficiency requirements our customers demand.”
Linaro and OpenDataPlane Project
Freescale is an active contributor to ODP, which is hosted by the Linaro Networking Group (LNG). Linaro is a not-for-profit organization consolidating and optimizing open source Linux software and tools for its members. The OpenDataPlane project was established within Linaro to produce an open-source, cross-platform set of application programming interfaces (APIs) for the networking data plane. ODP embraces and extends existing proprietary, optimized vendor-specific hardware blocks and software libraries to provide interoperability with minimal overhead. The project is open to contributions from all individuals and companies that share an interest in promoting a standard set of APIs to be used across the full range of network processor architectures available. For more information visit http://www.opendataplane.org.
About Freescale
Freescale Semiconductor (NYSE:FSL) enables secure, embedded processing solutions for the Internet of Tomorrow. Freescale’s solutions drive a more innovative and connected world, simplifying our lives and making us safer. While serving the world’s largest companies, Freescale is also committed to supporting science, technology, engineering and math (STEM) education, enabling the next generation of innovators.www.freescale.com
Freescale, the Freescale logo and QorIQ are trademarks of Freescale Semiconductor, Inc., Reg. U.S. Pat. & Tm. Off. All other product or service names are the property of their respective owners. All rights reserved. The Power Architecture and Power.org word marks and the Power and Power.org logos and related marks are trademarks and service marks licensed by Power.org. ARM is a trademark or registered trademarks of ARM Ltd or its subsidiaries in the EU and/or elsewhere. All rights reserved. © 2015 Freescale Semiconductor, Inc.
Freescale Semiconductor
Jack Taylor, 512-560-7143
jack.taylor@freescale.com
or
Gloria Shiu, (85-22) 666-8237
gloria.shiu@freescale.com
or
Laurent Massicot, (33-16) 935-7712
Laurent.massicot@freescale.com
or
Anjali Srivastava, (91-120) 395-0000
anjali.srivastava@freescale.com
or
Katsutoshi Furue, (81-3) 5437-9242
Furue.katsutoshi@freescale.com
Source: Freescale Semiconductor