Press Release

Media Alert: NXP at IMS 2019: Showcases Leading Technologies for 5G Wireless Infrastructure Innovation

May 17, 2019 at 9:00 AM EDT

Boston, MA – May 17, 2019 – At IMS 2019, NXP Semiconductors is helping to lead the way in 5G wireless infrastructure technology, smart antenna solutions and RF energy. Demonstrations include a full line-up of integrated solutions for 5G mMIMO cellular base stations, 5G mmWave solutions including high performance analog beamforming ICs in frequencies ranging from 24-40 GHz designed for both FWA and RAN applications, 5G macro solutions of RF power amplifiers and more. With more than 50 years of innovation, NXP's RF solutions, including RF transistors and mobile and infrastructure LNAs enable power levels and frequencies from milliwatts to kilowatts and frequencies from sub-6 GHz up to 40 GHz, the company is paving the way for cost-effective, highly integrated 5G systems.  

When:
Tuesday, 4 June                        09:30 to 17:00
Wednesday, 5 June                   09:30 to 17:00
Industry Hosted Reception         17:00 to 18:00
Thursday, 6 June                      09:30 to 15:00

Where: International Microwave Symposium, Boston Convention and Exhibition Center (NXP Booth# 548)

Media Event: NXP Unlocks Innovation for 5G Wireless Infrastructure
Get a deeper dive of NXP latest technology innovations helping to drive the future of 5G wireless infrastructure. This session is open to press and analysts. Registration is required.
When: Tuesday, June 4, 1:15 – 2:00 p.m. Eastern Time. Onsite check-in begins at 1:00 p.m.
Where: Boston Convention and Exhibition Center, NXP meeting room 209 on Level 2
» Press and analysts may register for the event by contacting, tate.tran@nxp.com.

NXP Showcase at IMS 2019: The Microwave Hub
Stop by the NXP booth where the company will showcase “The Microwave Hub” various 5G wireless infrastructure demos of cell tower base stations. Visit the NXP booth# 548 to explore the possibilities of integrating more functions into a single device.

Note to editors: To arrange an editorial meeting with NXP during IMS please contact Tate Tran, tate.tran@nxp.com or 408-802-0602.

About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ: NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better, and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy, and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has approximately 30,000 employees in more than 30 countries and posted revenue of $9.41 billion in 2018. Find out more at www.nxp.com.
NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2019 NXP B.V.

For more information, please contact:                                                  

Americas

Europe

Greater China / Asia

 

 

 

Tate Tran            

Martijn van der Linden

Ming Yue

 

 

 

Tel: +1 408-802-0602

Tel: +31 6 10914896

Tel: +86 21 2205 2690

 

 

 

Email: tate.tran@nxp.com

Email: martijn.van.der.linden@nxp.com

Email: ming.yue@nxp.com