“We’re extremely excited to be ramping the LPC84x family into production together with our broad base of customers,” said
Advancing its power-efficient integration and providing increased flexibility to developers, the LPC84x family builds on its innovation with a unique way to configure the device without CPU intervention. Upon power-up, its fast access initialization memory (FAIM) allows the clocks of the LPC84x microcontroller to be started in a low frequency mode, keeping startup current consumption to a minimum. Additionally, its input/output (IO) ports can come up immediately and in its desired configuration, eliminating any potential termination issues with attached devices, such as MOSFETs.
Within the LPC84x family, the LPC845 offers an additional flexible capacitive touch-sensing solution, which can operate in sleep and deep sleep modes, allowing for very low power performance. The LPC845 solution has been designed to handle up to nine capacitive buttons in different sensor configurations — such as a slider, rotary or a button matrix — along with supporting software libraries and tools to support additional features, including auto-calibration for best performance in noisy or wet environments, reducing false triggering. Evaluation kits and software packages available starting in Q3 2017.
Building on NXP’s global success of the LPC800 series, and keeping consistent with its proven, industry-leading innovations, the LPC84x family includes its powerful 32-bit State-Configurable Timer with PWM, advanced DMA, autonomous serial interfaces and patented IO switch matrix, where any peripheral function can be assigned to any of the 56 GPIO, enabling low-cost PCBs.
NXP’s new LPC84x MCU family offers developers a path to 64 KB of integrated flash memory and 16 KB SRAM, with a 12-bit ADC, dual 10-bit DAC, and a selectable output free-running oscillator (FRO) — further expanding the LPC800 series of feature-rich, entry-level MCUs at aggressive 8-bit pricing. Customers benefit from the family’s greater levels of integration for monitoring, data collection, sensing, real-time control and graphic interface capabilities, enabling basic control and connectivity tasks across a broad range of consumer, industrial and emerging IoT applications.
Pricing and Availability
Available in a scalable family of packages, including LQFP64, LQFP48, HVQFN48 and HVQFN33, the LPC84x MCU family of devices, along with supporting peripheral drivers, example software and tools, including the LPCXpresso845-MAX development board (OM13097), are available beginning
For pricing, please contact a local NXP sales office, and visit nxp.com/LPC84x for additional information of the LPC84x MCU family.
LPC Microcontrollers Demonstration
NXP will share its latest features and developments for the LPC portfolio at NXP FTF Connects in
About
NXP and the NXP logo and are trademarks of
For more information, please contact:Americas Tate Tran Tel: +1 408 802 0602 Email: tate.tran@nxp.comGreater China /Asia Esther Chang Tel: +886 2 8170 9990 Email: esther.chan@nxp.comEurope Martijn van der Linden Phone: +31 6 1091 4896 Email: martijn.van.der.linden@nxp.com