Press Release

NXP Introduces Modular IoT Gateway Solution with Multi-Protocol Compatibility for Secure, Reliable Wireless Connectivity in Smart Cities and Smart Industries

November 8, 2016 at 8:01 AM EST
NXP’s secure solution offers maximum design flexibility with broad connectivity options and NFC commissioning for quick deployment.

MUNICH, Germany, Nov. 08, 2016 (GLOBE NEWSWIRE) -- NXP Semiconductors N.V. (NASDAQ:NXPI) today unveiled a Modular IoT Gateway Solution for large node networks (LNNs) with pre-integrated, tested and RF certified support for a wide array of wireless communications protocols including Thread, ZigBee and Wi-Fi. This range of capability allows developers to easily build out gateways based on this solution, using their choice of wireless protocols for end-to-end wireless communications in LNN configurations with supporting cloud options such as Amazon Web Services (AWS).  

NXP Modular IoT Gateway
Top angle view of NXP's Modular IoT Gateway.


A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/408757d1-2b13-4f34-b728-47ef6b3b4272

Operators of smart commercial buildings and smart industrial environments deploying massive mesh networks need to be able to commission, control and monitor thousands of end nodes. Built on a fully-supported, open source Linux platform running on the latest i.MX processors, the robust Modular IoT Gateway addresses this demand by connecting Thread and ZigBee-based end node devices securely with the cloud through Wi-Fi or Ethernet. In addition, local intelligence enables time critical responses and operation even when cloud connectivity is not available. 

“With over 15 years of experience working with demanding wireless industrial as well as automatic meter reading and automatic meter infrastructure large node network applications, we learned that network security, flexibility, interoperability, scaling and robustness are critical to LNN commercial success,” says Robert Assimiti, Co-Founder and CTO of Centero. “Consequently, for Centero's emerging innovations using Thread for LNN applications such as lighting, we are basing designs on the NXP Modular IoT Gateway Solution.”

Robust Security for Protecting IoT Devices

The Modular IoT Gateway Solution addresses stringent network security requirements to protect user and system data through encrypted wireless communications which prevents unauthorized access, as well as interception, man-in-the-middle and replay attacks. Thread-based devices are authenticated to the network through the EC-JPAKE DTLS protocol which prevents passphrases from being leaked or reverse engineered. Thread and ZigBee messages use AES encryption for base level security at their respective mesh network layers, while offering flexible support for applications to add additional end-to-end security layers.

The Modular IoT Gateway also provides access to the advanced security capabilities of the i.MX application processor, including high assurance boot (HAB), secure key storage, secure JTAG, external tamper detection for passive and active events, and internal tamper detection for voltage, glitch and differential power analysis protection. Encryption software including OpenSSL is accelerated via the Cryptographic Acceleration and Assurance Module (CAAM). Trusted Execution Environment (TEE) support is available as an NXP Professional Services Product.

Simplified NFC Commissioning for Large Node Networks

Commercial installations with thousands of nodes can leverage the built-in secure NFC tap-and-connect capabilities through the gateway. Using a smart phone application, end nodes can be quickly and securely commissioned to the network, even when the device that is being installed is not powered, which is common in smart buildings and industrial, as well as smart connected cities, oil and gas fields and agriculture installations.  

A Complete Solution for Quick Deployment

NXP’s complete Modular IoT Gateway reference design includes critical building blocks for quick customization and application deployment including production ready hardware, schematics, bill of materials and fully documented software. Designers can evaluate, develop, prototype, iterate, field test, install and maintain LNNs for commercial settings starting with the Modular IoT Gateway Solutions platform.

“The IoT revolution is driving new requirements for our customers, and pushes the limits of their design teams,” said Denis Cabrol, director of global marketing for NXP’s microcontroller business line. “With NXP’s Modular IoT Gateway, it’s possible to develop secure and connected applications within months, without the need to hire a team of connectivity and security experts.”

Modular IoT Gateway - In Action at Electronica 2016
NXP will be demonstrating the Modular IoT Gateway with an animated ZigBee and Thread controlled Lighting Grid emulating an industrial environment at Electronica in Munich, Germany at the NXP booth located in Hall A6-107, November 8th – 11th.  Featured capabilities will include:

  • LNN lighting array highlighting simultaneous real-time multicast control of ZigBee and Thread edge nodes based on NXP wireless microcontrollers

  • Smart App used to control and commission LNN through the gateway

  • NFC No Power network commissioning of edge nodes via Smart App and Gateway

  • Modular design leveraging common radios across Gateway and Edge Nodes

  • Speech recognition control through Amazon Tap to AWS cloud

Availability
NXP’s Modular IoT Gateway is available now along with supporting documentation and quick start materials. As an extension to customer development efforts, NXP offers professional support and services along with support from Volansys, NXP’s expert connectivity partner. For more details and to learn how to buy, visit the NXP Designs reference library at nxp.com/modulargateway.

About NXP
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 44,000 employees in more than 35 countries and posted revenue of $6.1 billion in 2015. Find out more at www.nxp.com.

NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2016 NXP B.V.

For more information, please contact: 

Americas
Tate Tran
Tel: +1 408-802-0602
Email:tate.tran@nxp.com

Europe
Martijn van der Linden
Tel: +31 6 10914896
Email: martijn.van.der.linden@nxp.com

Greater China / Asia
Esther Chang
Tel: +886 2 8170 9990
Email: esther.chang@nxp.com

Primary Logo