EINDHOVEN,
Radar is a core advanced driving assistance (ADAS) technology for both traditional carmakers focused on automated driving levels 1-3 and for mobility as service innovators developing robotaxi and safe delivery applications for levels 4 and 5 automation. NXP’s new suite of radar sensing solutions meet both scenarios and provide a dedicated and optimized approach with critical scalability and design re-use to help carmakers address the needs of their diverse brand and model portfolios. This flexibility enables performance tailoring for the appropriate use case, reduces R&D effort and can speed up time to market.
NXP is enabling the ongoing evolution of radar with 2 new solutions.
New NXP Imaging Radar Solution
Imaging radar is a groundbreaking technology that significantly enhances radar’s performance. It delivers multi-modal capabilities and extends today’s available L2+ features, like highway pilot and lane change assistance, by offering super-resolution images for precise environmental mapping and scene understanding. This enhanced “understanding” is an important part of enabling full autonomy in urban settings where vehicles and vulnerable road users create driving complexity.
The combination of NXP’s new purpose-built S32R45 radar processor and the TEF82xx transceivers delivers the fine angular resolution, processing power and range required to not only distinguish between small objects in the distance, but also to accurately separate and classify vehicles and vulnerable road users like cyclists or pedestrians in crowded environments. This imaging capability aims to deliver better driving decisions.
NXP Scalable Corner and Front Radar Solution
Targeting cost-effective and small footprint NCAP corner radar requirements for high volume vehicle production, the NXP solution also provides scalability for long-range front radar and advanced multi-mode use cases like simultaneous blind-spot detection, lane change assistance and elevation sensing. These advanced applications require extended range and significantly enhanced angular resolution for detecting and clearly separating multiple objects simultaneously and provide the ability to surround the car in a 360-degree safety cocoon. NXP’s new S32R294 radar processors combined with the NXP TEF82xx transceivers provide a scalable solution that helps carmakers address both NCAP and advanced corner radar as well as long-range front radar sensor requirements in an effective way, while allowing tailoring for individual use cases.
“Radar has evolved from just detecting other cars’ velocity and distance to providing imaging radar’s high-resolution object and feature detection for precisely mapping the car’s surroundings,” said
As the first company to broadly deliver 77GHz RFCMOS radar technology in high volume mass production and as the developer of the groundbreaking S32 automotive processing platform, NXP stands alone in helping its customers optimize their total cost of ownership with maximum scalability and re-use across different radar systems, thereby optimizing their own R&D efficiency.
New NXP Radar Sensor Solutions are built on market-leading and volume-proven 16nm FinFET and 40nm RFCMOS technology. To learn more about NXP’s new RFCMOS 77GHz radar transceivers, the new S32R45 high-performance radar processors for imaging radar and the S32R294 radar processor for corner and front radar applications visit www.nxp.com/radar. NXP’s Radar Solutions are now sampling with customers and will be available in mass production during 2021.
CES 2021
Get a sneak peak at NXP’s CES 2021 as CTO
About NXP Semiconductors
NXP and the NXP logo are trademarks of
For more information, please contact:
Europa | ||||
Jason Deal | ||||
Tel: +44 7715228414 | Tel: +86 21 2205 2690 | |||
E-Mail: jason.deal@nxp.com | E-Mail: ming.yue@nxp.com |
A photo accompanying this announcement is available at https://www.globenewswire.com/NewsRoom/AttachmentNg/9a07a64e-73d5-444a-ae12-7752fcaf2781
Source: NXP Semiconductors N.V.